(free) 877-910-2094847-930-5118847-622-8766sales@helukabel.com
CompanyProductsQualityNewsContact usService
 You are here Home  Photovoltaik: SOLARFLEX®-X PV1-F

Photovoltaik: SOLARFLEX ®-X PV1-F

Using the brand name SOLARFLEX ®, HELUKABEL ® offers a wide variety of different wire types with VDE and TÜV approval, which were especially developed for the use in photovoltaics systems and which are immediately available due to an ex-stock delivery.


Photovoltaics systems produce direct current electricity by using several photovoltaics modules. Especially high safety requirements apply to the cables that connect the individual modules and the modules with the inverter. An electrical arc hazard exists in case of a short circuit. This is why our SOLARFLEX ®-X PV1-F is always delivered with a dual design of insulation and liner (crosslinked special compound).

Our solar cable is characterized by an extreme robust and abrasion resistant liner (required if the cables rub on the bricks or the metal edges of the substructure). An excellent UV, ozone, weather and hydrolyses resistance combined with an outstanding oil and chemicals resistance guarantee a long service life.

More information can be found in our new brochure Cable systems for photovoltaics.
  Download the new brochure

 HELUKABEL world-wide

www.helukabel.com
© 2007-2010 webmaster@helukabel.com