Production – Cable Production in Germany, Poland & China
HELUKABEL has been manufacturing cables since 1988 in the Windsbach factory near Nuremberg, the location where our cable production first began. Our test facilities are in the same location, and to date, Windsbach's production capacity has been expanded three times, which is a strong commitment to Germany as a production location. Other production plants in Europe are located in Meissen / Germany, and Jaworzno / Poland. Since 2024 in Changzhou, a production facility was established in China, which enables us to react quickly and flexibly to requests from Asian customers.
Windsbach & Meissen - Production Sites in Germany
In our two facilities we manufacture according to the latest production methods, and annually we produce approx. 1 million conductor kilometres (that’s 77 times around the globe). Over 300 employees are specialized in making high-quality standard and specialty cables.
Using the latest materials in cable technology, and cooperating with international testing institutes, makes us an innovation leader in the areas of automation, data technology, building management systems, and renewable energy.
Production figures:
- 65,000 m² Production facility
- 26 Extruder facilities
- 20 Stranding machines
- 60 Braiding machines
- Cables & wires from 0,05 to 1000 mm²
- According to: EAC, UL-CSA, HAR, CCC, Germanischer Lloyd, TÜV or according to customer specifications


Automation at the Windsbach Plant
Since 2024, a collaborative robot (cobot) has been supporting employees in mounting parts onto the specialised, automated machines.
The cobot inserts empty spools into the winding machine and removes them again after being wound. This allows the employees to concentrate on more important tasks.
In the following video you can gain an insight into the work of the cobot.
Jaworzno - Production in Poland
In the vicinity of Krakow, HELUKABEL Eltron manufactures high-quality copper stranded wires and strips, compensating and thermoelectric cables as well as cables withstanding high temperatures, for permanent use up to 400°C. The products, which are manufactured according to international standards as well as customer-specific requirements, are used worldwide, for example, in the automotive industry, electrical industry, large-scale plant construction and heavy industry sectors.


Changzhou - Production Site in China
At the beginning of 2024, the new HELUKABEL production facility in Changzhou, China, went into operation. With this ultra-modern production and logistics facility covering an area of around 25,000 square metres, we are significantly expanding our capacities in the People's Republic and will in future be able to offer our customers in and around China an even faster and more comprehensive service.