Magical Christmas Lights at Wilhelma

HELUKABEL supplies connection cables for the Christmas Garden in Stuttgart

Christmas Lights at Wilhelma

Along a two-kilometre circular path, elaborate and impressive installations invite visitors to be amazed and linger. (© Christmas Garden)

From 18 November, visitors of Stuttgart's Wilhelma can enjoy a truly magical experience: This is when the Christmas Garden in Stuttgart opens its doors again - one of the city's most popular attractions at Christmas time. As dusk falls, the grounds are transformed into a magnificent glittering world of over ten million lights. On a two-kilometre-long circular route, elaborate and impressive installations with lighting, video projections and music invite visitors to be amazed and linger.

This unique spectacle is possible thanks to a cooperation with HELUKABEL: we supplied several kilometres of H05RN-F , a connection cable for the installation of the sound systems, which also make the Christmas Garden an acoustic highlight. This harmonised rubber cable is characterised above all by its weather resistance and is therefore ideally suited for outdoor use - even in wet or freezing temperatures. Even more, these cables are also used at the Christmas Garden in Hanover and on the flower island Mainau in Lake Constance. The reliable technology ensures an optimal visitor experience!

The Christmas Garden in Stuttgart is open from 18 November 2021 to 16 January 2022 from 17:00 to 22:00.

Tickets and further information are available at www.christmas-garden.de .

Illuminated christmas garden in Wilhelma Stuttgart
More than ten million lights transform Stuttgart's Wilhelma into a magnificent glittering world, the Christmas Garden. (© Christmas Garden)
Back