Take Inventory at Record Pace

Save time and money by taking inventory of cables and wires using Aufmaster

Detailpicture of Aufmaster and the Aufmaster App

For most companies, the end of the year is inventory season, and this usually means cumbersome and time-consuming work. This is especially true for cables and wires that are stored on drums or in rings, are in lengths of hundreds of metres, and aren't easily measurable. Taking an exact inventory is therefore difficult - unless you have the right helper at your side.

The HELUKABEL portfolio has just what you need with the Aufmaster. This system consisting of a cable length measuring device and cloud-based software provides industrial, commercial, and craft businesses the ideal solution for simplifying and accelerating the inventory-taking process for stored cables and wires. The idea behind it is the stuff of genius. The Aufmaster measuring device is connected to the end of a cable with two clamps. It doesn't matter if the cable is wound or not. Then, the device measures the length of the cable using a patented measuring technique. This measurement is automatically communicated to the associated Aufmaster App. The user can easily view and save all measured cable lengths using a tablet or smartphone - all without having to wind any cables.

The app transfers the data in real time via the internet to the company account with Aufmaster. The cloud-based software controls and organises different projects, inventories, and multiple measuring devices installed on different cable drums. Inventory progress can be followed and documented live. What does this mean for you? Less work and more time for other tasks.

The Aufmaster measuring device is designed for cable diameters starting from 0.25 mm², and can detect lengths between 10 and 1,500 metres. With the Aufmaster App, even other high-volume items and consumables can be inventoried. The Aufmaster system is an efficient, uniform, and innovative system for taking the stress out of inventory season at your company.

Have we piqued your interest?

Learn more at aufmaster.de or in the HELUKABEL Online Shop!

Back