Cable Inspection with AI - nLine sets the standard in quality assurance

nLine's AI-assisted, visual quality control systems offer a 360°, real-time surface analysis, which presents a significant advantage in the manufacturing of cylindrical products such as cables, pipes, or hoses. Pascal Schwindhammer, Head of Equipment at HELUKABEL, and Hubert Eberle, Head of Sales at nLine, discuss how an inspection system grew into a company.

Nline cable inspection

nLine can analyse different surfaces, diameters and structures at production speeds of up to 500 m/min.

What exactly is nLine all about?

Hubert Eberle (nLine): nLine is a highly modern and innovative 360° inspection system for optical quality assurance. It was developed specifically for customers utilising continuous production processes to manufacture cylindrical products such as cables, pipes, wires, cords, or hoses. The system monitors the entire surface of the product in real time and immediately detects any abnormalities. This increases the level of quality, optimises process security, and makes the highest precision and efficiency possible.

Pascal Schwindhammer (HELUKABEL): nLine's precision and adaptability are one of a kind. For example, the system detects surface abnormalities such as scratches and tears and, with the help of AI, learns which abnormalities are tolerable and which are not. Even the most complex product surfaces, such as multicoloured, intricately woven cords, can be analysed with the highest accuracy. nLine is also able to be seamlessly integrated into existing production systems via field bus systems such as PROFIBUS or OPC UA. We are continuously developing nLine in order to flexibly react to customers' individual needs.

And what does this have to do with HELUKABEL, Mr Schwindhammer?

Schwindhammer: As nLine was still in its infancy, we developed a custom inspection system together with the experts from our production facility in Windsbach. Everyone involved contributed their expertise allowing us to come to a practical and future-proof solution that not only works quickly and precisely, but also detects and categorises mistakes swiftly. We had previously trialled and tested several systems in our production facilities before finally landing on the perfect solution in nLine. This digital quality inspector makes it possible for on-site experts to take any necessary corrective measures in order to maintain high quality standards. We see exciting potential in this partnership with nLine where we both profit simultaneously from each other's expertise.

Nline cable inspection system
Easy Setup:Teach new systems with a "Gut-Muster", or training sample, in mere minutes.

What makes nLine so special?

Eberle: In addition to the especially high-quality detection of anomalies, the system is defined by its particularly easy setup and operation. Furthermore, this inspection system is installed in the production line. The system is then taught with a so-called "Gut-Muster", or training sample, and immediately knows which specific product characteristics it needs to look for. On-site product training takes less than ten minutes, with analyses beginning immediately after. This AI-aided analysis allows data to be locally and quickly processed inside the device, which saves time, improves data security, and does not require a cloud connection.

Schwindhammer: This exact combination of AI, real-time monitoring, and flexibility allow us to detect and classify defects as early as possible, and to evaluate them according to tolerance ranges – all this before the cable even makes it to the drum. Reaching speeds of up to 500 metres per minute, nLine is also suitable for high-output production and functions with virtually no maintenance required, which is a significant advantage for users.

How did the idea for nLine even come about?

Eberle: Originally, nLine was a product of the company Wahtari, specialists in AI-based image recognition and automation. It was quickly clear that the quality assurance systems available at the time were not sufficiently efficient and did not offer 360° monitoring. Our vision was to develop a system together with HELUKABEL that works within the production process, is completely dependable, smart, and performs at the highest level. This is how nLine developed from a product into a company.

Does this mean that you originally worked for Wahtari, Mr Eberle?

Yes, exactly. I worked in sales at Wahtari and participated in the initial development of nLine. It was self-evident that I would take the product with me to the new company.

With nLine, what visions are now pursuing?

Nline cable inspection

Fully Integrable Software and hardware from a single source – simple & seamless integration into even preexisting plant designs.

Eberle: We would like to establish nLine as a global brand, and with the support of HELUKABEL, we see immense potential in getting our systems into manufacturing lines around the globe. nLine is designed to be a dynamic, adaptive system that meets and overcomes the challenges of tomorrow. Currently, we are working on integrating more functions, for example the ability to recognise codes and imprints.

Schwindhammer: Together, we are pursuing the vision of making production processes smarter, more efficient, and more sustainable globally – and that with the highest of quality. We want to better utilise and strengthen the leading edge our product has over other available solutions, as this technology can benefit the industry enormously. I am curious, and excited, to see what the next steps in development are.


Pascal Schwindhammer

Head of Equipment at HELUKABEL, has been with the company since 2022. His primary focus is on comprehensively supporting Kabelmat, Aufmaster, and nLine.

Do you have any questions about HELUKABEL Equipment?
Pascal Schwindhammer will gladly assist you:

pascal.schwindhammer@helukabel.de or at +49 170 8560420

Pascal Schwindhammer from Kabelmat

Hubert Eberle

Hubert Eberle, Head of Sales at nLine, has been with the company since 2023. His focus is on sales and the development of the company.

Do you have any questions about nLine?
Contact Hubert Eberle directly at: hubert.eberle@nline.ai or +49 89 21543006.

Hubert Eberle from Nline

ABOUT NLINE

nLine is a high-performance, visual quality assurance solution that combines efficiency and precision in production. With this collaboration with HELUKABEL, combination of digital and industrial competence revolutionises production processes. Building upon Wahtari's many years of experience with AI, nLine now finds itself in a position to take quality assurance to the next level globally.

www.nline.ai

ABOUT WAHTARI

Wahtari has developed AI-based image recognition systems for quality control and automation processes since 2019. This company is optimising industrial processes with complete, custom hardware and software solutions. This Bavarian company is able to offer future-proof and efficient solutions thanks to deep learning and impeccable IT security. The nLine inspection system arose from this with a clear focus on improving the efficiency and precision of the optical quality assurance of manufacturing processes.

wahtari.io

Back