Setting the Course for Wind Energy

WindEnergy Hamburg, the world's largest and most important meeting place for the wind industry, is taking place from 27 to 30 September 2022. HELUKABEL is participating as an exhibitor and will present its high level of expertise as a partner for manufacturers and suppliers of wind turbines in hall B6 at booth 224.

Helukabel at the WindEnergy Hamburg 2022

HELUKABEL's portfolio for the wind industry includes all kinds of cables and wires that are applied to the main components of wind turbines. The product range includes, for example, lightweight and flexible aluminium cables that can be pulled into the tower in one piece, eliminating unnecessary cost-intensive connections, and pre-assembled class 2 aluminium conductors that can be pre-installed in the individual tower segments. Torsion-capable cables with a wide variety of insulation materials, voltage levels and cross sections from 0.5 to 400 mm² are also part of the range. These are tested in HELUKABEL’s test tower to ensure that they are ready for series production. Heat-resistant cables for generator connections and slip ring applications, Ethernet cables and bus technology for data communication, and pre-assembled fibre optic cables in many different versions and as plug-and-play solutions for quick on-site installation complete HELUKABEL's product range for the wind energy sector.

With this extensive product portfolio, HELUKABEL provides optimal solutions for onshore and offshore wind turbines as well as for the infrastructure cabling of entire wind farms. The company has been supporting customers in the wind power industry for decades and, as a development partner to leading manufacturers, is very familiar with different application scenarios and requirements. Cables and conductors can be designed to be resistant to seawater, oil, ozone or UV radiation, among other things. At its development and manufacturing sites, HELUKABEL not only designs customised solutions from scratch, but also tests them in its own laboratories. Many products are certified according to UL, VDE or other standards, so that the right products can be found within the range for every target market. All the above makes HELUKABEL a reliable supplier of cables, wires and connection technology for the wind industry.

You will find HELUKABEL at WindEnergy Hamburg 2022 in hall B6 at booth 224. Come and visit us!

Back