Connection Solutions for Photovoltaics

HELUKABEL exhibiting at Intersolar Europe. Visit us in hall A4 at stand 308!

Helukabel at Intersolar

HELUKABEL shows off the solar cable series HELUPOWER SOLARFLEX and more at Intersolar Europe 2024. (Source: HELUKABEL)

"Connecting Solar Business" - The doors to Intersolar Europe in Munich, the world's foremost trade show for the solar power industry, are open from 19-21 June 2024. HELUKABEL will be there as an exhibitor presenting a number of solutions for electrical connection technology that installers and operators can rely on to economically carry energy from the sun and other renewable sources to its destinations. You can find us in hall A4 at stand 308.

With the HELUPOWER SOLARFLEX series, the HELUKABEL portfolio contains multiple cables that are specifically designed to connect solar modules to one another as well as with power inverters. The HELUPOWER SOLARFLEX-X H1Z2Z2-K UL is new to the program. With this cable, HELUKABEL is the first manufacturer to offer a solar cable constructed according to UL 4703, which is an important criterion for markets such as the USA. This cable is also suitable for worldwide export thanks to its DIN EN 50618 and IEC 62930 approvals.

Another new innovation is the HELUPOWER SOLARFLEX-X PREMIUM. This cable is certified according to TÜV 2 PfG 2750 and is therefore suited for use in floating photovoltaic systems, or floating farms. This cable has an especially long lifespan and is suitable for international use thanks to its DIN EN 50618 and IEC 62930 approvals. These HELUPOWER cables are not only available in their proven, standard design, but also with special rodent protection made from a stainless-steel mesh. All variants are halogen-free, flame-retardant, and resistant to UV rays, ozone, weathering, and water.

The HELUKABEL portfolio of photovoltaics cables also contains earthing and medium voltage cables for connection and grid feeding, as well as fibreglass and data cables for networks and communication. Moreover, operators can get their hands on integrated cable management systems consisting of connectors, plugs, glands, casings, and tools, as well as complete, pre-assembled cable systems. This is how HELUKABEL supports the manufacturers, installers, and operators of photovoltaic systems in generating clean, sustainable, and renewable energy.

Interested? You can find HELUKABEL at Intersolar Europe 2024 in hall A4 at stand 308. We look forward to seeing you there!

Back