Our Growing Portfolio of Solar Cables
HELUKABEL exhibiting at Intersolar Europe. Visit us in hall C4, at stand 579!
"Connecting Solar Business" - The doors to Intersolar Europe in Munich, the world's foremost trade show for the solar power industry, are open from the 7-9th of May 2025. HELUKABEL will be there as an exhibitor presenting a number of solutions for electrical connection technology that installers and operators can rely on to economically transmit energy from the sun and other renewable sources to their destinations. You can find us in hall C4 at stand 579.
With the HELUPOWER SOLARFLEX series, the HELUKABEL portfolio contains cables that are specially designed to connect solar modules to one another as well as with power inverters. Our HELUPOWER SOLARFLEX-X H1Z2Z2-K UL is constructed according to UL 4703, which is important for markets such as the USA. This cable is also suitable for worldwide export thanks to its DIN EN 50618 and IEC 62930 approvals. Some new additions to the program are the SOLARFLEX-X RPVU90-AL and SOLARFLEX-X RPVU90-CU variations with aluminium and copper conductors. These are constructed according to both UL and Canadian CSA C22.2 No 271 standards.
Another highlight is our HELUPOWER SOLARFLEX-X PREMIUM . This cable is certified according to the TÜV 2 PfG 2750 and is therefore suited for use in floating photovoltaic systems, or floating farms. It has an especially long lifespan and is suitable for international use thanks to its DIN EN 50618 and IEC 62930 approvals. These HELUPOWER cables are not only available in their proven, standard designs, but also with additional, special rodent protection made from stainless-steel mesh. All variants are halogen free, flame retardant, and resistant to UV rays, ozone, weathering, and water.
The HELUKABEL portfolio of photovoltaics cables also contains earthing and medium-voltage cables for connections and grid feeding, as well as fibre-glass and data cables for networks and communication. Moreover, operators can get their hands on integrated cable management systems consisting of connectors, plugs, glands, casings, and tools, as well as complete, pre-assembled cable systems. This is how HELUKABEL supports the manufacturers, installers, and operators of photovoltaic systems in generating clean, sustainable, and renewable energy.
Have we caught your attention? You can find HELUKABEL at Intersolar Europe 2025 in hall C4, at stand 579. We look forward to seeing you there!